iglidur on tour adventures continued: Pune to Bagalore (4000Km)

Post navigation

iglidur driver himself, Sascha, continues to give us his hands-on insight into the all around the world tour:

The Indian igus office is based in Bangalore, which is where we are now. We took a direct route from Pune to Bangalore which was, by the way, the longest we had so far. All in all it took us about 17 hours.

Bangalore is the capital of Karnataka and with about 8,4 million inhabitants, the third largest city (following Delhi and Bombay). Furthermore, it is the Silicon Valley of India. Although, it is further south, it is not as hot as Pune (nevertheless, still 30 degrees and sufficient for a painful sunburn).
As the following day was a Saturday, we kept it a bit slower with customer visits and made only five in total. One of the customers was Dynaspede.

They manufacture electro-mechanical components and machines for a wide spectrum of industries. You tell them what machine you want and they build it for you. We had the chance to get an insight view in an engine-testing machine, which is designed for a leading Indian car manufacturer, analysing the performance of engines.

They need to fix and move the engine. For this they put the engine on four shafts that are embedded in bearings.
Originally, they made use of THK bearings (Japanese company). At this time, they were facing many problems with scoring marks. Scoring marks are scratch marks on the shaft that are owed to movements. They occur when the friction between shaft and bearing is too high. To diminish this problem, they always had to lubricate as well as to use a hardened shaft. Eventually, they tried our Drylin® R FJUM-01-30 Flange housing instead, take a look at the igus flange housing for yourself: http://bit.ly/1hltyAD.

We supplied them directly with shafts and bearings at the same time. This not only decreased their number of vendors and therefore their administrative work, but also helps save money. As our products are self-lubricating and maintenance free, they solved their problem of the scoring marks. Thus, they have been using Drylin® R for years. They got rid of annoying work besides the actual work and could save costs. Nowadays, they don’t need to pay for the hardening of the shaft and for lubricating any more.

Inside the testing rid the engine is lifted and fixed both vertically and horizontally. There we have supplied jsm-6065-50 and jsm-20-23-20 for servo actuator and ejector pin respectively (horizontally). Inside the testing station is a shaft that they put on the gears-shift lever of the engine. The shaft is then moving the shift. Through this they are enabled to measure the performance. This shaft is guided by iglidur® J, which is characterized by a low wear with shaft materials and a low coefficient of friction.

We could also see our e-chains®. They are used for guidance and protection for moving cables. Most of their machines are already equipped with them.

The last days were entirely under the banner of driving and customer visits. We made at least another 1000km and visited about 25-30 of our beloved customers. Yesterday, I checked how many kilometers we have covered so far. About 4000! And there will be about 700km more as we are heading tomorrow towards Chennai, the other automobile hub of India.
Thus, I kind of cannot present you incredible adventure trips. No beach, no jungle, no desert etc. Just highways that were in a very good shape. I even cannot tell so much about Bangalore, just that at first glance, it seems to be a very modern and nice city.

Next time I will tell you more about the tour again. We’ll have some time in Chennai to discover a bit of the city, the culture itself and to visit some nice places.

As always I will keep you guys up to date,

Yours, Sascha

For more information, go onto the igus website: http://bit.ly/1aiIKyf