Southern Manufacturing 2016

Post navigation

We will be at Southern Manufacturing show from the 9th – 11th of February 2016 showcasing several new cable and bearing products on our stand (N97).

One focus to our stand will be the new dryin® W linear guide system, which is constructed entirely of carbon fibre reinforced plastic (CFRP). Ideal for applications across the aerospace, automotive and medical industries, the drylin® W linear guide system is up to 60% lighter than a traditional steel rail system, and 40% less compared with, the ‘light’ alternative, an aluminium rail. This light weight system is available for travel lengths of up to 2 metres, allowing designers to develop a more cost-effective solution.

“This CFRP linear system is ideal for aerospace and motorsport applications where weight may constitute money, or where high dynamic movements are important, such as robots for manufacturing,” said Rob Dumayne, director at igus®. “In addition, the carbon drylin® rail is available as a completely metal-free belt drive system, which integrates plastic pulleys and xiros® plastic ball bearings, meaning these systems can be used without restrictions within X-ray equipment.

Another focal point will be the readychain speed 2.0. Whilst looking for a solution to reduce the amount of cable needed for a customer, igus® developed readychain®; a pre-harnessed energy chain with integrated attachment designed for fast swapping. As with the whole readychain® service, the manufacturer only needs to determine exactly what is required, and igus® will supply the energy chain fully assembled and ready to fit.

Come along and visit our technical experts from the igus® team who will be available throughout the show to provide visitors with practical advice and guidance on selecting igus® products for their own specific applications.

Baby feet in feathers