Automatic instant online pricing for 3D-printed parts in technical plastics

Post navigation

igus, the motion plastics specialist, has undertaken extensive research and development into 3D printing filament in order to offer its industrial customers more freedom in their product design and prototyping. The result was the world’s first technical plastic filament and SLS powder for use in 3D printing, designed specifically for moving applications. Customers can purchase the filament for use in their own 3D printers or specify and order parts direct from igus via its easy online ordering and 3D printing service, which now offers automatic instant pricing.

Using the tribo-filament, it is now possible to create 3D-printed plain bearings that deliver both form and function. 50 times more wear-resistant than conventional 3D printing materials, it was developed for engineers that need to create structurally robust prototypes or even small batch samples for real-world tests. The lubrication-free, abrasion-resistant iglidur 3D printing materials have exceptional strength, even when compared to parts made traditionally via machining and injection moulding.

The process of purchasing parts made with igus 3D printing materials is now even easier via the igus 3-step online ordering and 3D printing service:

  1. Drag and drop your .stl file into the igus configurator.
  2. With the 360° viewer, check your model and enter the units of measurement you require.
  3. Select a suitable material, your desired order quantity, and place your selection in the shopping basket to receive your instant price

“Thanks to 3D printing, the prices are competitive for making both prototypes and small batches for production,” says igus director, Robert Dumayne. “Depending on project complexity, completed 3D-printed parts can be delivered in as little as 24 hours.”

For further information about the online 3D printing service, please visit: www.igus.co.uk/3d_printeror call igus directly on 01604 677240. Follow us at twitter.com/igusUK, watch our videos at www.igus.co.uk/YouTube, connect with us at www.igus.co.uk/Facebook and read our blog on blog.igus.co.uk.

image.axd