xiros® is a trademark name by igus® and it is the name we give the umbrella of products that fall under the ball bearing umbrella. Historically, igus® was known for sliding bearings rather than the rolling balls found within a ball bearing, but after many years of material development and testing, the xiros® product group was launched in to the market. Within this range there are deep grove radial ball bearings, a range of axial ball bearings, thrust washers, slewing rings, labelling and conveyor rollers and we offer bespoke parts with integration of other components to keep costs and component count to a minimum.
xiros® bearings are offered by igus® and selected by our customers in order to solve application in either a cost effective way and / or a way that provides longer life over a plain bearing or metallic solutions. xiros® ,being made of polymer races and stainless, glass or polymer balls require no additional lubrication. We find that we have thousands of customers in the Food and Packaging, Automotive, aerospace and special purpose machine building industries.
We test the xiros® bearings extensively before, during and after a material is released. We apply multiple loads, speeds and sequences to determine the products life expectancy for a range of sizes and use this data to build our online ‘expert system’ to predict life for a customers application.
xiros® is made up of several components. If we just focus on the radial deep grove ball bearings, they are made up of a moulded inner race, moulded outer race and a moulded cage. We then assemble with either a stainless steel, glass or polymer ball depending on the application. The design of the assembly is so that we are able to snap the bearing assemblies together and yet they still offer huge strength under axial and radial loading and can’t become dismantled in application. All moulding and assembly happen in our factory in Cologne alongside our plain bushing, spherical and linear bearings being moulded and assembled. We can make bespoke solutions in high volumes using this same method and for lower quantity solutions we can machine using our plastic rod / stock bar material. There is no MOQ.
The xiros® range covers many different types of bearings:
- deep groove ball
- flanged ball
- thrust ball
- pillow block
- slewing ring
- ball transfer units
- conveyor rollers
Other special designs are available so find out more on the xiros page.
Many of our xiros® materials are FDA-approved, find out more on the website.
All of the xiros® bearings are long-lasting, but each material and design will produce a unique service life. Use the service life calculator to find out how long-lasting each bearing is.
xiros® bearings are being used in myriad industries and applications, some examples are:
- bicycle wash system – low absorption means powerful operation
- pellet stove – high temperature properties ensure no melting
- pool cleaner – deep groove ball bearings ensure steady operation
- labelling machines – self-lubrication means smooth running
- ball bearing races on both sides of the ball bearings
- ball bearing cage
- different ball bearing types: stainless steel, glass, polymer
The beneficial properties include:
- corrosion-resistance
- underwater applicability
- lubrication-free
- maintenance-free
- ESD-compliant
- FDA-compliant
- lightweight
- high media resistance
- high and low temperature applicability: -100°C to +150°C
- metal free or metal-detectable
- predictable service life
You can use the xiros® expert for guide rollers. This requires some simple inputs such as diameters and lengths, along with load and speed. The system will give you a list of suitable parts given the inputted information. Click on the link.
We calculate the lifetime of the roller through the xiros® ball-bearings lifetime. This can be easily calculated using the xiros® life-time calculator. Click on the link.
The bearings can be easily removed from the roller tube and replaced.
We can supply a bespoke solution to suit your application- please discuss with our expert to determine the optimum solution. Call us on 01604 677240 or visit the website for more information.
We can supply shafts in all materials, from aluminium to stainless steel. Shafts can be supplied as a standard length or machined to suit with additional threads/keyways etc. There is a configuration tool to help. Click here.
As with all igus® solutions the xiros® rollers require no additions lubrication. This makes them particularly suitable for the food or packaging environment.
The xiros® rollers are available as a FDA version with conformity to regulation 10/2011/EU and regulation 1935/2004/EC Please find the link to the BBT-PVC30 here:
Yes We Can – we would need to discuss the application in detail with you, looking at the overall speeds and loads to determine if a longer roller can be produced. Please ring the office on 01604 677240 to discuss options!
Please click the form here and we will respond within 24 hours to discuss your application with you. We can visit physically or arrange a virtual meeting. You can also call the usual number 01604 677240 to be put through to our specialist.