the-chain®

e-chains®, or energy-chains, protect and guide moving cables and hoses. They go by a lot of names: cable carrier, cat track, drag chain and power-chain. They are usually made of plastic and occasional out of metal, though this has some drawbacks.

igus® readychain® systems are e-chain® systems supplied complete with cables, hoses, connectors and even custom metal work.  This allows them to be fitted quickly and easily to your machine, saving time and money.

igus® readychains can be supplied at 4 levels:

  • readychain® basic: energy chains supplied with cables and hoses installed and cut to length
  • readychain® standard: energy chains supplied with cables and hoses installed, cut to length complete with required connectors fitted and electrically tested
  • readychain® standard plus: energy chains supplied with cables and hoses installed, cut to length complete with required connectors fitted and electrically tested with optimised connection points / interfaces
  • readychain® premium: one or several energy chains supplied with cables and hoses installed, cut to length complete with required connectors fitted and  electrically tested, supplied on a transport rack for easy transport and installation

There is certain basic data that is required – the diameters, weights and minimum bend radius data for the cables and hoses. Also, the application data, such as machine travel length, speed, acceleration and even the environmental conditions. Service life calculations can be obtained with our online tool here.

At igus®, we have online expert systems to help which offer the available options for these inputs and show respective lifetimes and costs.  Of course, we can also support by phone, email, Livechat and visits to your site by our sales engineer team.

The longest in service now is a travel length of 615m, which has been running trouble-free for 10 years. We are confident we have the products that will reach 800m travels and beyond.

Use the e-chain® calculation tool here.

igus® also offers a full range of dynamically rated cables for use in constantly flexing applications (“chainflex®“), which are guaranteed for 10 million movements or 36 months when used as per our guidelines. These can be supplied with or without connectors and pre-fitted into the energy chains. We also offer steel and aluminium guide troughs for longer travels, cable clamping solutions for cable strain-relief and chain interior separation options to ensure a long cable life inside the chain.  We also offer design and project support, onsite services such as supervision and inspection and full turnkey installation.

igus® e-chains®, or energy chains, can cope with fill weights of up to 600 kg/m unsupported.

igus® can carry out offshore surveys on existing chains, and also offer full turnkey installation, or installation supervision, on any of our chains being installed offshore.

igus® e-loop has been designed to enable the operator to replace single cables/hoses in situ, rather than having to replace the full service loops. The e-loop is built up in links, which can be opened to allow the cables to be changed. The dyneema rope which runs through the middle of the e-loop is pre-tensioned to the working load, and so takes the strain of the cables or hoses in use.

Yes! igus® e-loop is supplied with an industry-standard mounting bracket and flange, as per on major OEM top drives, so it is a simple and quick retrofit!

igus® has thousands of energy chains on existing applications offshore including cantilever skids, pipelay towers, gantry cranes, and many more as seen here. Our polymer energy chains are maintenance-free, corrosion resistant, and cost effective vs equivalent steel chains.

Yes!

igus® can carry out offshore surveys on existing chains/cable management solutions and retrofit them with a new maintenance free igus® energy chain! We offer a complete turnkey engineered solution to suit our customers’ requirements!

Yes, igus® has cables for many industries, including offshore. Our cables with DNV/GL & NEK606 certification can be found and investigated here.

Although igus® does not manufacture hydraulic hoses, the hoses can be sourced and installed within your e-chain® to your requirements.

Our online tool prevents our customers from over filling the e-chains®. We have recommendations for the amount of clearance each service should have when installed within the e-chain® (relative to its OD); 10% for all round and flat cables, 5-10% for pneumatics, 20% for hydraulic hoses and 15-20% for all other media hoses.

  1. ready to install: all readychain® systems are assembled at one of the worldwide igus® factories
  2. lifetime guarantee: all readychain® components undergo extensive checks through quality and functional tests
  3. reduce the number of your suppliers by 75%: lower project planning expenditure and increase efficiency
  4. flexible production plans: state of the art technology to ensure optimised production
  5. safeguarded and short delivery times: our experienced and consistent team guarantees customer satisfaction for high quality at low costs

The limiting factor would be how large the drum is with this chain wrapped around, and the lifting gear required to handle on site, but we are regularly delivering systems for travels of 100m and beyond; these can be split mid length too for a smaller diameter drum.

Almost every industry with moving energy needs use e-chains®: cranes, lifts, theatres, vessels, machine tools, renewable energy systems, electronics, pick-and-place machines, telescopes, agriculture, printing, vehicle sliding doors, and so on – the list is endless.

The maximum is currently 80M. 

4M/S

Absolutely!

10 million cycles, or 10,000km is our guaranteed statement

 

No, a visual inspection is required every 6-12 months and adjustment of cable tensions (if necessary)

88% faster installation time than standard chain

All igus® energy chain sensors (push/pull monitoring, abrasion, motion, wear measurement, break detection) can be connected to an icom or icom. plus module. The module can transmit the measurement data to an equipment monitor or a computer, where they are displayed individually or in a dashboard.

No, you do not need that. In monitoring their own production, every entrepreneur can decide for himself how much he wants to digitise and utilise the opportunities offered by the Internet of Things. Not everyone is already connected and not everyone wants to network.

Many are concerned about transferring their sensitive company data to external servers, even if high security standards are guaranteed. However, if you use the isense online system from igus, to synchronise and keep data up-to-date, the installed module connects directly to the igus server and sends the data anonymously. The company’s own network remains unaffected at all times.

Companies who still prefer to run their production monitoring offline, i.e. without Internet connection and permanent data update in their own operating system, can certainly do so. They install systems that give a warning in case of defects or simply switch off the machines via normally closed or normally open contacts to prevent major damage and breakdowns.

Such sensors for energy chainscables and bearing technology, such as the sensor for break detection on e-chains EC.B, run autonomously and have a great effect with low installation effort.

No, you do not have to. If your organisation wants to monitor production and switch to predictive maintenance, you do not have to buy extra hardware and set up a new IT infrastructure.

The prerequisite for the most accurate information possible on the trouble-free running time of our components is that the details of use given by the operator are accurate. This includes information on the place of use with weather conditions and temperatures, distances, loads, number of cycles, etc.

When computers and machines learn from collected data and derive an action from it, one speaks of Artificial Intelligence (AI). The term machine learning is also used in the machine sector.

In private life, one example is that of users of music streaming services. Here an algorithm constantly learns from the behaviour of the user

With CF.Q, CF.D and CF.P, igus has three sensors in the product range that are designed for chainflex cables.

CF.Q is the sensor for the electrical specifications of chainflex cables

  • Belongs to prevention of crash and can be used without an additional module
  • Indicates changes in the electrical properties
  • In the event of a fault, information by means of NO contact or message

We have a configurator tool and a product finder tool which both will help you specify the energy chain required. Click here for the product finder.

Click here for the configurator tool

The automotive guarantee is a service that igus® offers to ensure that the systems are installed correctly, therefore enabling the 36 month guarantee to be awarded for both chain and cable. 

There are 3 options which you can find information about here: https://www.igus.co.uk/info/automotive-guarantee

 

Yes. We recommend the TH3 energy chain, which has been developed specifically for the food and beverage industry.

Yes, all igus energy chain materials can be deployed in continuous use at temperatures as low as -40 °C.

Yes, the autoglide system allows travels of up to 80 m without guide troughs.

Yes, plastic energy chains that use the igumid HT material can resist swarf as hot as + 850 C.

detailed list provides information on the resistance of igus’s igumid G, TE, and NB materials to many chemical substances.

As a rule, the standard temperature range for plastic energy chains is -40 °C to +130 °C, short term +170 °C.

Read More

Issue 10/2019

Autumn is here and the UK engineering exhibition season starts with Advanced Engineering, again at the NEC, on 30th and 31st October 2019. You will find igus® on stand H8, where we plan to have all 2019 new products on show and VR headsets where you can fly through the igus® factory. As always, we will have engineers on hand to talk you through the products, and we will be serving drinks and light refreshments all day.

Read More




Tech up. Cost down. It’s our job

People’s ability to adapt their way of living has become second to none. Not being able to exhibit in the normal fashion hasn’t stopped igus® from showcasing their new products. They have introduced a virtual exhibition. The blog explains how you can visit from the comfort of your home office!

Read More


Slewing ring systems

iglidur® PRT slewing ring bearings combine igus®  polymers with high quality hard anodised aluminium rings.  The maintenance-free sliding elements are manufactured from proven tribologically optimised iglidur® materials. The rings are lightweight anodised aluminium or corrosion resistant 316 stainless. 

These offer many advantages over metallic roller and ball bearing alternatives. They are fully configurable on our website as well as being life calculable. We can provide the CAD for any part and once ordered, are delivered ready-to install. These parts are self-lubricating and offer very low wear all environments.

The belt profiled outer options make driving these slewing rings easy, we have a range of belt options to chose from including AT10, T10, HTD5M and HTD8M. Spur gearing is favourable for simple direct drive.

There are endless opportunities for these PRT slewing rings, in all kinds of applications and some of the key features are:

For example:

Completely maintenance-free
Easy to install and replaceable sliding elements
High wear resistance
For very high loads and high stiffness
Stainless steel versions available
Extensive accessories available, such as hand clamps and position stops.
FDA options available
Bespoke and full integration enquires welcome

The PRT slewing rings are used in multiple of industries. Furniture manufacturers, Material handling, Food and Packaging to name a few.

We call our slewing rings the PRT range.

There are currently 4 ranges, PRT-01, PRT-02, PRT-03 & PRT-04. Each have a variation of sizes from 20mm-300mm dia. 

PRT’s can be mounted horizontally and also vertically so very adaptable. 

Yes, the PRT-01-20-C is equipped with a collar clamp

Yes the PRT-04 is approx 25% less than the PRT-01 version. 

Yes we do. Ours is ESD Compliant and comes with maintenance free sliding elements out of iglidur® F2. The part number is PRT-01-XXX-ES-F2

We have various accessories:

Manual clamps, drive shafts, distance ring, the individual gliding pads, clamping level, adaptor plate, angle stop sets. Please click here to see all available accessories. 

For use in ESD or ATEX areas, we recommend using iglidur® PRT slewing rings with stainless-steel rings and sliding elements made of iglidur F2.

Yes. As an option, iglidur® FDA-compliant PRT slewing rings with iglidur® A180 plain bearings and stainless-steel rings are available.

This depends on the size of the slewing ring. The maximum permissible load on the currently largest iglidur PRT, PRT-01-300, is 150 kN statically in an axial direction, which corresponds to a weight of 15 t. During movement, the permissible load is 90 kN. For the smallest model, PRT-02-20 – for applications with small loads and simultaneously high pressure of costs –, the maximum load is 13 kN statically and 4 kN during movement.

The maximum speed depends on the size. For the largest possible iglidur PRT slewing ring, PRT-01-300, this is 50rpm; for the smallest, PRT-01-20, it is 300rpm.

The square version is for very high loads and offers a high rigidity. It is easy to install and makes replacing the sliding pads easy.

The PRT-04 ESD has iglidur® F2 sliding elements which avoids the electrostatic charges. It is stainless steel so conductive and protects against electrical currents. 

The new PRT-04-50-T is a new slot nut profile PRT which allows add-on parts to be added and mounted retrospectively. Perfect for the medical industry 

i-sense is the smart bearing technology which allows production monitoring making it “predictive”. The sensors can be operated as a stand alone system or can be integrated within the production infrastructure. 

With the PRT range, the sensor measures the abrasion of the sliding elements and alerts when there starts to have wear allowing you to replace before the part starts to fail.

Read More