Carnival in Rio de Janeiro
Once a year, usually in February, Rio de Janeiro turns into the biggest carnival party in the world. Every day there are around two million people on the streets with the main attraction being the colourful parade that is filled with revellers, floats and adornments from numerous Samba schools.
 
The Samba schools are competing against each other not only in dancing but also in playing drums, creativity of costumes etc. The parade only goes through a certain street. Thus, you must buy a ticket if you wish to see it. For those not able to get one, cameras are recording everything, some are remote controlled and can move a few hundred meters along the parade. In the picture below you can see a rail for cameras at the top of the stage.
 
This rail is equipped with a 320 meter long cost-efficient DryLin® rail that ensures the smooth, noise-free motion of the cameras. See here for more Drylin information: http://bit.ly/1fljKqg
 
DryLin® WS 28 guarantees that no camera sticks whilst moving with speeds up to 60km/h. The TV channels have been relying on our rail for about four years. While doing this, the rail has been unprotected throughout the entire time and had to face rain, sun and incredibly high humidity. A diverse range of environmental conditions and of course, it still works perfectly.
Example of DryLin® W rail for cameras: