Fire and Ashes
When you travel thousands of kilometres, it is important that the seat is robust and comfortable. iglidur® bearings enable the driver to maintain a comfortable sitting position. Worldwide, manufacturers are using igus products to improve their seating in vehicles.
A seat manufacturer from Japan, who makes use of iglidur®
Seating manufacturers make use of iglidur® in several elements including seat height adjustments, backrest angle adjustments, crash-active headrest and adjustment motors.

iglidur® bearings are convincing with smooth motion. We make use of iglidur® for the seat in our car too. Our bearings help adjusting the seat without making any noise.

Although it can be said to be dependant on the weight of the person, the bearings must endure a high static load. With 100N/mm² iglidur® bearings could even carry the heaviest sumo wrestler. However, the quality of being able to carry a heavy weight does not compromise on the weight of the bearing itself; they remain light (about seven times lighter than conventional metal bearings). They are a cost-effective and reliable bearing solution for any kind of seat.
Japan comprises of four large islands, of which includes the mainland with Tokyo and Hiroshima. From Hiroshima we travelled right to the southern island Kyushu.


Kyushu is the third largest island, famous for its numerous hot springs. Pillars of white steam can be seen everywhere. Hot springs seem frequent, whilst we were in Taiwan, one of our bearings we immersed in boiling hot spring water for more than one hour, the result; the bearing was no different to before it went in! The clouds you can see in the background are not those of the usual kind, yet from hot springs in the mountains.

The unique geography of Japan (being situated at the edges of three tectonic plates), encourages the high percentage of springs. Here, the Pacific Plate, Philippine Plate and the Eurasian Plate are meeting, resulting in Japan not only a centre for hot springs, but also to one of tsunamis and active volcanoes. As our bearings can easily endure high heat (For instance: iglidur X is suitable for temperatures of +250 °C (long-time) and up to +315 °C (short-time), we took the car to Mount Aso; not only the largest active volcano in Japan, yet one of the contenders among the largest in the world. As the soil near a volcano is very fertile, the surrounding is very green.


Already from far away, while passing the lowland below the volcano, you can see the pillar of smoke.

The last eruption of Mount Aso was in 2011.

An eruption at our visit would have been surely more dangerous for us than our bearings. They are all dirt and heat resistant.

From Mount Aso, we travelled North again where we passed a chain of small islands near the mainland.


From there, we drove straight about 800 kilometres to the coastal city Nagoya.

In Japan, we have already coveredabout 3000 kilometres.
I will keep you up to date,
yours Sascha.