How to calculate tensile strength 

Tensile strength is a critical material measurement, especially in engineering and design. It measures the maximum amount of tensile (pulling) force a material can withstand before breaking. Understanding how to calculate tensile strength is essential for ensuring the safety and reliability of structures and components. In this blog, we’ll walk you through the steps to calculate tensile strength and explain the key concepts involved.

How to calculate tensile strength 

What is Tensile Strength? 

Tensile strength is the maximum stress that a material can endure while being stretched or pulled before breaking. It is typically measured in units of force per unit area, such as Pascals (Pa), Megapascals (MPa), or pounds per square inch (psi). 

Key Concepts 

Before we dive into the calculation, let’s clarify some important terms: 

  • Stress: The force applied to a material divided by the cross-sectional area over which the force is applied. It is measured in units of force per unit area (e.g. N/m² or psi). 
  • Strain: The deformation or elongation of a material in response to an applied stress. It is a dimensionless quantity, representing the change in length divided by the original length. 
  • Elastic Limit: The maximum stress that a material can withstand without permanent deformation. 
  • Yield Strength: The stress at which a material begins to deform. 

Safety first! 

Ensuring safety during tensile testing is crucial. Before you get started, here are some key safety guidelines to follow: 

  1. Check equipment: Before starting the test, inspect the tensile testing machine for any signs of wear or damage. Ensure all components are functioning correctly. 
  1. Proper alignment: Make sure the specimen is properly aligned in the grips to avoid slippage or misalignment during the test. 
  1. Use protective gear: Wear appropriate personal protective equipment (PPE) such as safety goggles, gloves, and lab coats to protect against potential hazards 
  1. Limit switches: Verify the placement of limit switch rings to prevent the machine from exceeding its operational limits 
  1. Regular maintenance: Perform regular maintenance checks on the machine, including tightening the V-belt drive and checking for wear and tear 
  1. Emergency procedures: Familiarise yourself with the emergency stop procedures and ensure they are easily accessible during testing 

Steps to calculate tensile strength 

  1. Prepare the material sample: Obtain a sample of the material you want to test. The sample should have a uniform cross-sectional area and be free of defects. 
  1. Measure the original dimensions: Measure the original length (L₀) and cross-sectional area (A₀) of the sample. Accurate measurements are crucial for precise calculations. 
  1. Apply tensile force: Use a tensile testing machine to apply a gradually increasing tensile force (F) to the sample. The machine will record the force and the corresponding elongation of the sample. 
  1. Record the maximum force: Continue applying the force until the sample breaks. Record the maximum force (Fₘₐₓ) that the sample withstands before breaking. 
  1. Calculate tensile strength: Use the following formula to calculate the tensile strength (σₜ): 

σt=FmaxA0σt​=A0​Fmax​​ 

Where: 

  • σtσt​ is the tensile strength. 
  • FmaxFmax​ is the maximum force applied. 
  • A0A0​ is the original cross-sectional area. 

Example calculation of tensile strength

Let’s go through an example to illustrate the calculation: 

  • Original Length (L): 100 mm 
  • Original Cross-Sectional Area (A): 10 mm² 
  • Maximum Force (Fₐₓ): 5000 N 

Using the formula: 

σt=5000 N10 mm2=500 N/mm2=500 MPaσt​=10mm25000N​=500N/mm2=500MPa 

So, the tensile strength of the material is 500 MPa. 

Calculating tensile strength is a fundamental process in material science and engineering. By understanding and applying the steps outlined in this blog, you can determine the tensile strength of various materials and ensure their suitability for different applications. Remember to follow safety guidelines and use appropriate equipment when conducting tensile tests. 

If you’re keen to learn more, why not explore our range of ‘How to’ blogs

You may also like...