Yukon & British Columbia
Where have igus parts been used within the car? Find out here: http://bit.ly/1uWKWUU
We have started our journey into the Yukon, driving along the famous Alaskan Highway. The Yukon is known for its miles and miles of undisturbed wilderness, which includes many species of animals, countless lakes, creeks, and other unexpected surprises along the way.

The Yukon Territory is the shape of a right triangle, bordering the state of Alaska. There are very small towns and villages along the way, with hours of driving in between. We spoke with some local people, one man told us that he was sick and had to drive over twenty-three hours to the closest hospital. There is also very limited internet and cell phone reception in these towns, so if anything were to happen, you have to use your resources – a survival of the fittest lifestyle is important when living in an area like this.

The iglidur car has travelled miles and miles through rocky, muddy, winding roads. Many other vehicles many have broken down, but the iglidur car has had no problem travelling through these conditions. Surely this is because of the iglidur bearings we had retrofit into the car, like iglidur G in the brake pedal.

iglidur G is the all-around (the world!) performer, excellent for most applications; maintenance-free, self-lubricating, wear-resistant, and cost-effective. It is resistant to dirt and dust, which is all the car has seen since it arrived in Alaska!

We’ve made a few stops in Whitehorse and WatsonLake over the 3 days it took us to drive through the Yukon. Along the way, we were able to see a mother black bear and her 3 cubs…

As well as a heard of antelope, wild horses and bison, a porcupine, multiple moose, and a reindeer! It was amazing to be able to see these animals completely surrounded by their natural habitat.


There are so many hidden gems in the Yukon. One of the highlights for us was the hot springs in Liard, which is the second largest hot spring in Canada.

This hot spring is unique, as the hot springs are on one side, so on that side, the water is extremely hot, but cools down as you move further away. We swam in the hot spring for over an hour – just the relaxation we needed after 3 longs days of driving.

As we headed out of the Yukon and into the Rocky Mountains, we left behind the gravel roads and found ourselves surrounded by turquoise rivers winding for miles along massive mountains. But, as usual, this was no challenge for our iglidur car as it continued cruising through winding, twisting roads up into the cliffs. While the car is still running great without any problems, the exterior is looking a little rough. What started out as a bright orange on arrival in Alaska has now turned a light brown!
The iglidur Car with the Rocky Mountains
Keep your eyes peeled for us in Vancouver, where we’re heading next!

We will keep you up to date,
Yours Sascha