Tribo Tape

Tribo Tape

Please accept cookies to play this video. By accepting you will be accessing content from a service provided by an external third party.
Accept

 

Get tribo-tape now!

 

Tribo-tape transcript  

“Hello, Rob Dumayne here again, dry-tech Director for the UK. I just want to introduce you to our new tribo-tape materials. These are tribologically enhanced materials that are low friction. Varying from the V400 which is a high temperature material, the B160 material which is a black low friction, high wear material, the W160 which is an anti-UV material, so that means we can have that out in the daytime in direct sunlight and it won’t affect the properties of the material, and finally, the A160 which is a food approved, low friction, self-adhesive tape. 

So, this is just an example of very simple shape which we can cut out.  We have a simple square, or a kidney bean shape for a wear strip on a conveyor system and even special stamped out pieces which we can produce at a very high volume as well. If you do a lot of repetitive work with self-adhesive, low friction tape, then this is the material for that. This one also comes on a large reel, which you can buy by the metre or on a 50m reel. All available from stock in all the 4 materials mentioned earlier. 

So if you would like more information, please contact us on the info below, and we will be able to get some samples out to you.” 

 

86 views

You may also like...