The CFRIP range is extended to over 230 cable types
“Long lengths can be stripped in half the time and the system ensures that no damage occurs to the core insulation,” says James Harrison, chainflex Product Manager at igus.
The outer jacket can be stripped to the desired length simply by pulling the special CFRIP cord, a fast and effective way of stripping cables.
Along with chainflex CF5 PVC control cables, where the CFRIP cord is in the outer jacket, and the shielded version chainflex CF6, where the cord is in the inner jacket – CFRIP is now integrated in the CF130 and CF140 control cable family, as well as the entire motor cable range.
Want more information?
Visit the igus website on http://bit.ly/1g6z1LF
Or contact James himself on:
jharrison@igus.co.uk/ 07971 468439