106 Search Results

For the term "robot".
slewing ring bearings

Ever tried putting a round bearing in a square hole?

Slewing rings are such versatile products and with a varied range, the igus® PRT slewing rings open up many doors which would ordinarily be closed. Read all about the uncomplicated slewing rings and visit the new PRT page on the website to see the full range.

Did you know that igus® sells flexible cables?

Being one of the worlds largest energy chain manufacturers, it makes perfect sense for us to be growing the cable side of the business and yet very few people even know that igus® sells cables!

Forget chocolate vending machines, introducing mask vending machines!

When you think of vending machines you think of chocolate, crisps or drinks. When you think of a dispenser you might think of a grab machine you find in arcades that potentially could bankrupt you before you have successfully won a toy! But 2020 has bought us the mask vending machine and igus® has the perfect product to go inside.

e-spool® – the alternative to a cable drum

Having to work with small installation space can be a challenge but with the igus® e-spool system space limitations is not a problem. This system comes as a motorised option and can be fully equipped with igus® cables.

Cost-effective e-chains®

it is essential that there is a range of cost-effective energy chains on the market. These are ideal for industries such as furniture and office equipment. igus® has some very clever cost-effective e-chains®….

Tell me more about igus® dryves

igus® dryves are the motor controllers that we have developed to help customers reach a complete solution. Mainly, they consist of the igus® D1 dryve, this is the stepper motor controller we have, which can also control brushed and brushless DC motors. Then, we have the igus® D3 dryve which is a simple brushed DC motor controller for simple applications. This basically represents two sectors: the D1 dryve as an industrial controller for cartesian robots, delta robots and articulated robot arms, including those produced by igus®.

The fairy tale of the finest stranded wire

A conductor is the part of a wire that is responsible for the current flow. So, the copper in the middle is covered by the insulation so that the current does not get into the neighbouring wires. If the conductor consists of more than one wire, according to our strand specialist. While several wires form a strand, a strand covered with insulation represents a wire.