For more information about igus® plastic rods visit igus.co.uk/plasticrod.
What is the standard length of a plastic rod?
The standard length of the stock bar is 1000mm long.
Can we sell by the mm?
We can sell by the mm in both plate and bar materials – prices are on request for the stock plate however. you are able to get prices for stock bar online. Please click here.
Can we machine parts to drawing?
Yes we can. All we need is a PDF and if possible a CAD file. You can upload your requirements on this form.
Can we supply machining guidelines?
These are supplied on the product page at the bottom under the technical data. Please click here.
Which are the best tools to machine igus® stock bar?
iglidur® materials are easily machined with tools manufactured in HSS (High Speed Steel). You can also use hard carbide metal. All tools need to be sharp.
What is tempering?
Tempering is a term for heating up material to relieve tension in the material. All of our iglidur materials are tempered. Should you wish to temper igus material please adhere to the following;
The heating process needs to be conducted slowly due to the low conductivity of the material. The specific temperatures should be reached in approx 3-4 hours by heating slowly from room temperature. This allows for even and consistent heating. The given temperature should be maintained for 1 hour per 10mm wall thickness.
The cooling process must be done slowly to avoid tension in the material. The rate that the materials should be cooled at a rate of 20 °C per hour max.
Tempering temperatures;
iglidur J, J4, A180, R, A181, J2, J3, J200 – 120 °C
iglidur J260- 130 °C
iglidur W300, P210- 180 °C
iglidur A350-J350, H1- 200°C
iglidur x- 220°C and hold for 2 hours per 10mm wall thickness.
Why do plastic rods come slightly oversized?
This is to allow the customer to precision ground to the diameter required.
What diameters do igus® stock bars come in?
Currently our largest range is iglidur J and this ranges from 10mm dia right up to 100mm dia. We can offer iglidur J tubes which have a larger outer diameter. The majority of the other ranges come in at least 4 or 5 different diameters as minimum.
What size does the igus HLW come in?
This is currently available in 30mm diameter. The standard length is 1000mm but can be cut to increments of 100mm.
Is HLW FDA compliant?
The HLW material does not have FDA compliance.
How do I know which stock material is the best for my application?
We have the stock bar material finder available on our website! You can find it here.
It allows you to put the parameters and requirements of your application and specifies the best material.
Does igus® sell standard plastic bar?
We only sell igus® ranges so only iglidur stock materials. We have a large range and can provide like for like with the standard materials such as Acetal, Nylon, PET
Does igus® offer FDA materials in plastic rod or plate?
We have a large range of FDA materials in both rod and plate. We have high temperature materials such as A500 or AC500.
We also have less high performance materials such as A160 and A180 which are also FDA approved, hard wearing but lower in costs as the temperature range and chemical resistance is not as high as the likes of A500 and A350.