chainflex

Cable designs and why chainflex® cables are superior

There are a vast range of calves that are available on the market. So why would you pick an igus® cable over a competitors? What can happen if the relationship between cable and chain is not stable? Let’s find out….

Hard or soft cable for e- chains®: which is best?

No matter whether you call the energy chain an e-chain® or a drag chain, it also does not matter whether cables have Flexible Dynamic (FD), highly flexible (HF) or “chain” in the name. For the user, it is not the name that matters, but rather the function and durability.
This question about gut feeling is often answered. It usually says: “Soft hugs well” or “hard breaks much faster”. But what is actually right?

The fairy tale of the finest stranded wire

A conductor is the part of a wire that is responsible for the current flow. So, the copper in the middle is covered by the insulation so that the current does not get into the neighbouring wires. If the conductor consists of more than one wire, according to our strand specialist. While several wires form a strand, a strand covered with insulation represents a wire.

How does cable insulation protect from high temperatures?

The ambient temperature and electrical loads on the cable play a decisive role in the functionality and longevity of cables and connectors.
At least since the long forgotten hours of physics, we have known that electricity and heat are related. This connection is clear again and again when it comes to cables.
The consequences of high temperatures on your cables can have drastic effects on your production liens and your costs.

Which Ethernet cable is right for me?

It can be a minefield when trying to identify what type of cables you need for your application. igus® have a variety of cables and can help you decide which one is best for you.

Bus malfunction in cables paralyses production

The energy chain is considered the umbilical cord of machines with a moving application, whereby the cables act as nerve pathways. The line quality must permanently meet the requirements of the movement. The interplay between the energy chain and cables must match. What happens if this is not the case? We would like to illustrate in today’s blog article.

Single core vs multi-core motor cables for high-performance spindles

Motor cables more or less always have the same structure. Depending on requirements, single core or multicore motor cables are used. Both types of cables are suitable for high loads. So, what is the difference?
Spindle drives in processing and machine tools are becoming increasingly larger and more demanding in terms of performance and thus energy supply. As a result, larger cable cross-sections and thicker motor cables are required. To that end, however, the cables and the energy chain no longer fit into the existing installation space of the machine. The cables need to change.