dry-tech

How are plastic gears made?

How are plastic gears made?

Plastic gears are going to be the thing of the future. No lubrication, lightweight, recyclable but there is more. More options for you as the customer. igus® now machine, 3D print and mould gears in our iglidur® material. Which method would be best for you?

FDA bar stock

How can FDA bar stock material help your application?

igus® has a large range of FDA approved products, in both the chain range and the bearing. However occasionally the standard range might not quite fit the design so having a large range of stock materials enables customers to be as creative as they desire.

How to construct and assemble a spindle motor.

When people mention motors they assume that they are overly technical and difficult. igus® has a range of motors that are available from stock, easy to assemble and low cost.

bearings for binoculars

igus® protecting our shores through binoculars

Sometimes it isn’t about the “big” order. Sometimes it is about doing something nice. Helping the National Coastwatch Institute recently was so rewarding. Knowing that igus® bearings were helping them protect our shores was priceless.

Plastic bearings

What Are Common Misconceptions About Plastic Bearings

It is understandable that people have misconceptions surrounding the reliability of plastic bearings over metal bearings. But are these misconception’s justified or should I minds be more open to change?

Are your products cold resistant?

No one likes to be cold. However, there are some igus® products that not only cope with the cold, they thrive in it. This blog highlights but a few products that will withstand more than just the English winters, some of the products are capable of -40°C and some as low as -100°C……

Do I need to lubricate bearings if they are plastic?

Lubricating bearings can be a pain. It is not only messy but the grease can be detrimental in some cases to the machine. Thanks to the technology used within the material makeup of iglidur® bearings, igus® bearings don’t need any form of lubrication. No grease. No oil. Nothing.

What Applications Would You Use A Knife Edge Roller?

Knife edge rollers are used in so many applications however they are so overlooked as a product. At igus® we have a large range of iglidur® materials that are available as rollers. Find out more in this blog.