iglidur

bearings for binoculars

igus® protecting our shores through binoculars

Sometimes it isn’t about the “big” order. Sometimes it is about doing something nice. Helping the National Coastwatch Institute recently was so rewarding. Knowing that igus® bearings were helping them protect our shores was priceless.

Plastic bearings

What Are Common Misconceptions About Plastic Bearings

It is understandable that people have misconceptions surrounding the reliability of plastic bearings over metal bearings. But are these misconception’s justified or should I minds be more open to change?

Are your products cold resistant?

No one likes to be cold. However, there are some igus® products that not only cope with the cold, they thrive in it. This blog highlights but a few products that will withstand more than just the English winters, some of the products are capable of -40°C and some as low as -100°C……

Do I need to lubricate bearings if they are plastic?

Lubricating bearings can be a pain. It is not only messy but the grease can be detrimental in some cases to the machine. Thanks to the technology used within the material makeup of iglidur® bearings, igus® bearings don’t need any form of lubrication. No grease. No oil. Nothing.

What Applications Would You Use A Knife Edge Roller?

Knife edge rollers are used in so many applications however they are so overlooked as a product. At igus® we have a large range of iglidur® materials that are available as rollers. Find out more in this blog.

slewing ring bearings

Ever tried putting a round bearing in a square hole?

Slewing rings are such versatile products and with a varied range, the igus® PRT slewing rings open up many doors which would ordinarily be closed. Read all about the uncomplicated slewing rings and visit the new PRT page on the website to see the full range.

What is the difference between iglidur® and metal rolled bearings?

For years igus® has been asked if they sell metal rolled bearings. This blog is to explain why the iglidur® materials are not only better for your applications but also to show you how you can reduce cost, increase lifetime and help in our fight with a more sustainable world.